ISABELLENHUETTE (ISA) is the world's leading manufacturer of low-value precision resistors.In 1987, the company produced the first milli-ohm surface-mount current-sense resistor in the world and still holds the leading position in this technology. ISA is one of the world's leading manufacturers of thermistors and resistors for temperature measurement, used in the automotive, electrical and electronics industries. Low temperature coefficient, low thermoelectromotive force, good long-term stability, low parasitic inductance, high pulse load are the basic requirements for the precision resistor used for current detection. Some of these features are based on the properties of the resistive material itself, and some are determined by the design and manufacturing process.