EN
  • EN
  • DE

25 cents to achieve 25 different functions of the MCU, is it true?

Friday, December 1, 2017

Give you 25 cents, what can you buy? A subway ticket? not enough! An egg cake, at least three 25 cents, right? If you are an electronic engineer to give you a MCU only 25 cents, and can achieve 25 different functions, will not be excited? Yes, TI's recently introduced MSP430 is such a great value induction microcontroller, users want to achieve 25 different functions, just download different applications, it is worth mentioning that the cost is very low.

Image result for MSP430 MCU

Why MSP430 MCU better than the fixed integrated circuit?

Why MSP430 can achieve 25 kinds of functions? Media Conference Texas Instruments China MSP Microcontroller Business Development Manager Mr. Diao Yong give an answer.

First, the MSP430 enables easy programming with flexibility and scalability. Designers can customize common analog and digital functions for different applications by downloading different programs.

Second, the code can be reused, allowing designers to easily port functions to new designs or other MSP430 microcontrollers.

Third, low cost, only 25 cents for bulk costs and 25 different functions for high volume deployments.

Details MSP430 MCU 25 kinds of functions which can be achieved?

These 25 kinds of functions can be divided into four major parts, including: timer function, pulse width modulation function, system function, communication function.
Timer function:

External RTC with spare memory
7-segment LED stopwatch
External programmable watchdog timer
Programmable system wake-up controller
System wake-up controller based on real-time clock
The voltage monitor is equipped with a time stamp

Pulse width modulation function

Analog input, PWM output
Dual output 8-bit PWM DAC
Servo motor control
Stepper motor control
UART software controls RGB LED color mixing

System functions

ADC wake-up and transmit thresholds
EEPROM emulation
Low-power hexagonal button
Quadrature encoder position counter
Configure UART Hysteresis Comparator
Multi-function reset controller
Single-slope analog-digital conversion technology
Tamper detection
Programmable clock source
Programmable frequency lock loop

Communication function

Single wired host
SPI IO Extender
UART to UART bridge
UART to SPI bridge

The newest MSP430FR2000 from TI is the smallest MCU in this series. It has 0.5KB internal memory and is compatible with all other functions except MSP430FR2100 with 10-bit ADC and 1KB internal memory. The MSP430FR2110 and MSP430FR2111 all come with a 10-bit ADC , The former with 2KB memory, the latter 4KB. Several of the above have low-cost, small memory, less peripheral features. In addition to the following several low-cost memory outside the larger, more devices, such as MSP430FR2311 with 4KB of memory, transimpedance amplifier and op amp; MSP430FR2033, MSP430FR2433 and MSP430FR4133 except with 16KB of memory, 10 ADC, MSP430FR2033 60 IO interface. MSP430FR2433 package size is smaller, MSP430FR4133 integrated LCD controller.

TI also introduced the MSP430 LaunchPadTM new development kit, MSP-EXP430FR2433, based on the MSP430FR2433 microcontroller with integrated eZ-FET debugger and EnergyTraceTM technology.

To help you understand and use these features, TI has produced an electronic manual that contains 25 short application notes with source code links. Within minutes, it is possible to compile, download the source code and run on the MSP430 Value Sensing MCUs. Features can be adapted to your application needs, dramatically reducing time-to-market.

Author:Brittany Antonia (The author of article owns the copyright.)  

RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess