- IMB-M43H Sixth or Seventh Generation Intel® Core ™ Processor Optimized for Design with I / O Compatible
ADLINK Introduces IMB-M43H, a New ATX Industrial Motherboard with Excellent Compute Performance, Supports Generation 6 and 7th Generation Intel® Core ™ i7 / i5 / i3 Processors (Note) Compatible with Windows 7 operating system when using Gen 6 processors. In addition, support for multiple expansion slots and compatibility with various I / O allows the IMB-M43H to be integrated with machine vision and motion control, plus rugged I / O for immunity and radiosity certification to aid system operation The stability of the upgrade, is to create high-level automation system cost-effective choice.
ATX industrial motherboard IMB-M43H, supports the sixth generation / seventh generation Intel Core processor
Has excellent computing performance
ADLINK's ATX Industrial Motherboard IMB-M43H with the latest Gen7 or Gen 6 Intel® Core ™ i7 / i5 / i3 processors offers the advantage of multiple simultaneous motion control and visual processing, compared to the previous generation , Computing power increased by 10%, while the image performance even up to 30%. Qiu Xianguang, product manager of ADLINK Embedded Platform and Modules Division, said: "In order to maintain a computer-controlled automation system, factories and manufacturers spend a lot of resources to maintain system performance, time to market, and total cost of ownership. The company is the most important business challenge. "
"We took advantage of the powerful computing power of the latest generation of Intel processors to upgrade existing industrial automation computer systems while still supporting existing operating systems such as Windows 7, as well as compatibility with a variety of traditional I / O interfaces , Such as multiple PCI slots, PS / 2, COM port and VGA interface, and support for PCI Express x16 and x4 expansion slots, in addition to cost advantages, but also to meet the machine vision and motion control real-time operation needs, It is a cost-effective option for users in advanced automation applications. "
Integrate machine vision and motion control to give your automation application key capabilities
ADLINK IMB-M43H dedicated mainstream expansion slots, including a third generation PCI Express x16, a second-generation PCI Express x4, and five PCI expansion slots for the image acquisition card, digitizer, and high-resolution dynamic signal Acquisition and general-purpose modules, offering a variety of PCI Express expansion options; and diverse motion control and I / O modules enable real-time deployment of machine vision and industrial automation. From traditional machine automation applications to advanced industrial Internet of Things solutions, motion control, machine vision and automated optical inspection operations, how machines, people and businesses work together, and in the semiconductor and flat panel display industries Is playing a key and important role, the IMB-M43H is meeting this vital need and offers significant benefits for industrial automation applications.
ADLINK IMB-M43H also uses a superior level of reinforcement I / O to enhance the stability of the operation. Contains a unique power supply design that keeps each USB port stable at 5 volts and plus or minus 5%, allowing all USB ports to reach full load, even when power comes from a 300-watt power supply. In addition, immunity to IEC 61000-4-2 to IEC 61000-4-6 (Performance Criterion A) is guaranteed to ensure that I / O will not degrade during operation as well as to pass EN 55032 Class B-EMI radiation The certification ensures that the IMB-M43H reduces the amount of radiation up to 10 dB compared to most competitors.
ADLINK plowed automation industrial control applications for more than 20 years, with motion control, machine vision and measurement testing and other automation equipment manufacturing expertise and experience, to provide customers with rich products and complete services. IMB-M43H can be integrated and highly compatible with ADLINK's full range of image acquisition cards, motion controllers and data acquisition cards. Combined with efficient computing power, optimized design, and rugged I / O, we help customers reduce time-to-market and lower total cost of ownership.
By Clicking "Allow", you agree to the storing of cookies on your device to enhance site navigation, analyze site usage, and assist in our marketing efforts.
Country/Currency details