EN
  • EN
  • DE

ON Semiconductor Introduces World's First Extensible Next Generation Automotive Image Sensor Series

Friday, October 27, 2017

ON Semiconductor today introduced a new CMOS image sensor platform that combines automotive applications such as ADAS, mirror replacement, rear view and look-around system and autopilot, etc., to promote energy efficiency innovation and automotive image sensor market leader ON Semiconductor today. Performance and image quality to a new level. The HayabusaTM platform features a breakthrough 3.0-micron back-illuminated pixel design that delivers the industry's highest electronic charge capacity of 100,000 and has other key automotive features such as high-dynamic range (HDR), LED flashing (LFM) and real-time Functional safety and automotive certification.

"The Hayabusa series enables automakers to meet evolving ADAS standards, such as the European NCAP 2020, and provide next-generation features such as electronic rearview mirrors and anti-flickers," said Ross Jatou, vice president and general manager of ON Semiconductor's Automotive Solutions Division. Technology, the optical size of the sensor can be extended from 1/2 inch to 1/4 inch, reducing the time and work of customers to develop multiple automotive platforms, is conducive to speed up the product market. ON Semiconductor has been shipped this A pixel-oriented image sensor, a high-end digital camera for film production and television, and now we use this proven architecture for new sensors developed in accordance with automotive standards. "

This high charge capacity pixel design enables the Hayabusa series of each image sensor to provide super exposure, even in the most challenging scenarios, can also provide 120 dB (dB) HDR and LFM high-fidelity images, and not Will sacrifice low light sensitivity. Hayabusa Platform Synchronization The functionality of HDR and LFM is particularly important for improving safety, ensuring that all objects and potential hazards are identified in extremely dark and extremely bright scenes. With the LED widely used in headlights, taillights and traffic lights, Hayabusa platform LFM function to ensure that the pulse light will not flash to make the driver distracted; or applied to the front of the ADAS system, but also to avoid the machine vision algorithm Scene of the scene.

The Hayabusa product line also features real-time functional safety features that conform to the ISO 26262 standard, reminding the system processor of any problems or potential errors in the sensor. These features allow the system design to be rated to the Automotive Safety Integrity Level (ASIL-C). Real-time capability can instantly identify errors without waiting for a complete image to be transferred to the processor for image analysis. Faster response time allows the system processor to take immediate action to solve the problem, which is less than 100 seconds on the highway vehicle speed is essential.

Different for AR03 seriesAR01 series ,the Hayabusa series's first product is a 260-megapixel (MP) AR0233 CMOS image sensor capable of running at 60 fps while providing ultra-high dynamic range and eliminating LED flicker technology with all the features of the Hayabusa platform. Trailer customers can now apply for samples. For more information, please contact ON Semiconductor's sales representative.

Find more ON Semiconductor products

  Author :Brittany Antonia — WIN SOURCE ELECTRONICS

 (The author of article owns the copyright.) 

RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess