Give you 25 cents, what can you buy? A subway ticket? not enough! An egg cake, at least three 25 cents, right? If you are an electronic engineer to give you a MCU only 25 cents, and can achieve 25 different functions, will not be excited? Yes, TI's recently introduced MSP430 is such a great value induction microcontroller, users want to achieve 25 different functions, just download different applications, it is worth mentioning that the cost is very low.
Vishay Intertechnology, Inc. today announced the availability of the new series of automotive grade film chip resistors 0402, 0603 and 0805 - the MCS 0402 HP, the MCT 0603 HP and the MCU 0805 HP - with the industry's highest rated power consumption Scattered Vishay Beyschlag MC HP Series devices are used in electronics for automotive, industrial and renewable energy applications. They operate up to + 175 ° C and have a load life drift of less than 0.2% after 1000 hours of operation at nominal dissipation.
STMicroelectronics (ST), a leading global semiconductor supplier spanning multiple electronic applications, introduces the latest electronic innovations to make precision motor control for precision robots even more advanced.
Vishay Intertechnology, Inc. today announced the SiRA20DP, the new 25V N-channel TrenchFET® Gen IV power MOSFET that offers the industry's lowest on-resistance of 10V at only 0.58mΩ. With the lowest gate charge and less than 0.6mΩ on-resistance, Vishay Siliconix SiRA20DP minimizes the gate-to-on resistance product product of the value of the figure of merit (FOM), enabling applications to increase efficiency and power density.
With the 600 V CoolMOS ™ CFD7, Infineon Technologies AG introduces the latest high-voltage super-junction MOSFET technology. The 600 V CoolMOS ™ CFD7 is a new addition to the CoolMOS 7 family.
Melexis, a global leader in microelectronics, today announced the launch of a new line of miniature far-infrared (FIR) sensors for a wide range of applications requiring accurate temperature measurements.
Maxim announced the MAX86140 and MAX86141 optical pulse oximetry / MAX30001 heart rate sensor and an electrocardiogram (ECG) and bioelectrical impedance (BioZ) measurement analog front end (AFE) to provide effective solutions for preventive care and continuous monitoring products, wearable health support , Fitness application. These small size, low-power solutions enable high-precision vital signs signal measurement, monitoring health / fitness conditions, helping to prevent health hazards and strangling them to budding.
Maxim announces the DS28E38 DeepCover® Security Authenticator, an anti-physical attack solution that enables designers to easily and proactively secure proactive protection solutions at low cost, reliably protecting their intellectual property and products.
Artesyn Embedded Technologies announces the two new 15W and 20W DC / DC power converters, the AEE15W-M and AEE20W-M, to provide OEMs and manufacturers of industrial products and medical devices with a lower cost yet Power system solutions that meet the stringent requirements to ensure that these must be assisted or enhanced insulation system products are related to certification, in line with industrial products and medical equipment safety standards.
You may now have fixed-function integrated circuits (ICs) for a long time, and in some cases have adapted to their limited flexibility. A simple Universal Asynchronous Receiver Transmitter (UART) to Serial Peripheral Interface (SPI) bridge, a reset controller, or an external real-time controller (RTC) with back-up memory performs well in its own right, but But only for the set function.