EN
  • EN
  • DE

RSS

Blog

Today, Intel announces the Intel® Stratix® 10 MX FPGA, the industry's first field-programmable gate array (FPGA) with integrated high-bandwidth memory DRAM (HBM2). By integrating HBM2, Intel Stratix 10 MX FPGAs provide up to 10 times the memory bandwidth of a standalone DDR memory solution. With its powerful bandwidth capabilities, Intel Stratix 10 MX FPGAs can be used as basic multifunction accelerators for high performance computing (HPC), data center, network function virtualization (NFV) and broadcast applications that require hardware accelerators to facilitate large-scale data movement and Flow Data Pipeline Frame Speed.
Silicon Labs (also known as "core science and technology") has introduced a series of optical biometric sensors to provide advanced heart rate monitoring (HRM) and electrocardiogram (ECG) functions for a variety of wearable fitness and health products. The new Si117x sensor module offers ultra-low power consumption, high sensitivity and excellent integration, making it ideal for smartwatches, wrists, patch devices or other wearable devices that require long battery life and higher heart rate accuracy. To simplify development and reduce time-to-market, Silicon Labs offers a complete sensing solution that integrates the Si117x sensor module, heart rate algorithm, Wireless Gecko SoC with Bluetooth® connectivity, and an easy-to-use wrist with sample code, sample projects Development Kit. Silicon Labs will be simultaneously exhibiting Si117x sensor modules and complete solutions at the 6th Shenzhen Embedded Expo hosted December 21-23. Welcome to booth 1A08 of Hall 1 of Shenzhen Convention and Exhibition Center.
Melexis, a global microelectronics engineering company, announced the release of MLX90818, a new high-precision pressure sensor designed for demanding media applications in the automotive industry.
Developing radiation-tolerant systems for space applications requires not only long lead times but also very high costs because the system must be extremely reliable for long years in harsh environments. Today, NewSpace and other important aerospace applications require accelerated development and lower costs. To meet these needs, Microchip Technology Inc. has introduced a new microcontroller (MCU) that combines unique radiation resistance with the low cost development features of existing commercial (COTS) devices.
Diodes Corporation today introduced the AL1788, a worldwide leader and supplier of high-quality, application-specific standard products to a broad range of independent, logic, analog and mixed-signal semiconductor markets. This high-performance offline constant voltage combined with a PFC controller combines high power factor correction (PFC) with low total harmonic distortion (THD) with low standby power, making it ideal for commercial applications and networking lighting needs.
As more and more cars have networking and autonomous driving capabilities, the embedded messaging security of automotive communications becomes even more critical. Infineon Technologies AG and ESCRYPT Ltd. are working closely together in the field of automotive network security to deliver a solution designed to encrypt on-board communications and enhance communications while taking into account future security needs. The solution is based on Infineon's second-generation family of AURIX ™ (TC3xx) multicore microcontrollers and CycurHSM security software tailored by ESCRYPT.
Ams AG, a leading global provider of high-performance sensor solutions, today announced the AS39513, an NFC sensor tag and data logger IC that can be used in smart labels to enable the detection of food, pharmaceutical and healthcare Product storage and transportation in the process of more efficient and accurate monitoring.
Maxim announces the MAX14878, MAX14879, and MAX148802.75kV and 5kV family of isolated controller area network (CAN) transceivers to help designers improve industrial communication reliability and system uptime.
In recent years, hybrid vehicles and electric vehicles continue to evolve, and the demand for miniaturization, weight reduction, capacity increase, and high heat resistance of the mounted electronic components is increasing. Murata Manufacturing Co., Ltd. (hereinafter referred to as "Murata") and MHI Co., Ltd. (hereinafter referred to as "Matsushita Electric Works") jointly developed the FH series of high-temperature-resistant film capacitors that can be continuously used under a high temperature of 125 ° C. The product is ideal for environmentally friendly car converters and motor drive converters that require warmer temperatures in the future. Samples will be available starting in September 2017 and will be available in April 2018 at Murata's FMCG Solutions. Production.
Texas Instruments Incorporated introduces a new family of 4K Ultra High Definition (UHD) chipsets that continue to drive 4K ultra-high definition applications and technological innovations. Building on the industry's first affordable 4K UHD chipset, the DLP660TE, TI has introduced two smaller chipsets, the DLP470TE and DLP470TP, that continue to extend 4K Ultra HD to a wider range of end-use applications.
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess