EN
  • EN
  • DE

RSS

Blog

Melexis, the global leader in microelectronics technology, announces the second generation of a motor position sensor (resolver) based on its patented Triaxis Hall magnetic sensing technology. The next generation MLX90380 single-chip solution can be used to measure absolute motor angles for all brushless motors including Permanent Magnet Synchronous Motor (PMSM) and Brushless DC Motor (BLDC). The electrification of the car has given rise to the continuing growth of related applications, for which the MLX90380 offers the ideal solution.
TDK Corporation has expanded its lineup of chip varistors for automotive applications. The AVRH series has a maximum operating voltage of 19 V to 70 V and a capacitance range of 4.7 pF to 50 pF. This compact voltage protection device can be used in IEC 1005 (EIA 0402) due to its compact size of only 1.0 mm x 0.5 mm x 0.5 mm, which results in a 75% reduction in volume of new components over existing components with comparable performance, . The high reliability AVRH series is also available in an operating temperature range of -55 to 150 ° C and withstands 25 kV contact discharges in accordance with IEC 61000-4-2 and AEC-Q200 certified.
New Device and Feature-Rich Evaluation Boards Help Engineers Speed Development of Control Applications for Server, Communication and Industrial Markets. The new MachXO3-9400 devices combine the benefits of both on-chip memory and flexible programmable I / O in the MachXO3 product family, further enhancing support for complex applications that require more logic and embedded memory
Renesas Electronics (China) Co., Ltd. ("Renesas Electronics"), a subsidiary of Renesas Electronics Corp., a leading global semiconductor solution provider, today announced the release of the new RZ / N Series Industrial Networking Communication Microprocessor ) To simplify web-based application development. The RZ / N series is ideal for industrial network equipment such as network switches, gateways, programmable logic controllers (PLCs), operator terminals and remote I / O units.
The device improves the sensitivity to visible light, filters with infrared radiation suppression, and is packaged in a small size SMD package
Terence Semiconductor Corporation (Second Tokyo Stock Exchange: 6616) has developed a multi-chip module power IC that integrates four Schottky diodes and LDO voltage regulators.
Cypress Semiconductor Corporation (Nasdaq: CY) today announced that DENSO, a global supplier of automotive components and systems, uses the 6-channel Power Management Integrated Circuit (PMIC) for Cypress Automotive and FL-S serial NOR flash memory solution for the latest driving support system (ADAS) cast the latest stereoscopic vision sensor.
NXP Semiconductors (Nasdaq: NXPI, hereinafter referred to as "NXP") today announced the highest award for China's security and security, "Blue Shield Cup Security Technology Innovation Award" and "Blue Shield Cup security security market development award." "Blue Shield Cup" awards by the China International Science and Technology Promotion Association card swapping industry alliance and card card security technical forum Organizing Committee jointly organized by the relevant experts in the field of the final assessment committee.
Dialog will support Xilinx Zynq-7000 SoC, Zynq UltraScale + MPSoC and Spartan-7 FPGAs with an efficient, scalable, and flexible power management IC
The HayabusaTM platform provides 120 dB of ultra high dynamic range (UHDR) and eliminates LED flicker (LFM) imaging with 1 MP to 5 MP pixels for selection
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess