EN
  • EN
  • DE
RSS

Blog

Recently, Vishay Intertechnology, Inc. (NYSE: VSH) announced the launch of new conductive (184 CPNS, 185 CPNZ, and 186 CPNT series) and mixed conductive (182 CPHZ and 183 CPHT series) aluminum polymer capacitors with 4mm x A variety of frame sizes from 4mm x 5.5mm to 10mm x 10mm x 12.4mm. Vishay BCcomponents capacitors have longer life than standard aluminum capacitors, and they also have higher ripple currents and better impedance, saving PCB space and reducing costs.
On April 10, 2018, Analog Devices (ADI) announced the introduction of the Power by LinearTM LTM4661, a low power step-up μModule® regulator in a 6.25mm x 6.25mm x 2.42mm BGA package.
The 5kW power supply is housed in a 1U high, 19" (483mm) wide rack mount package and has the highest power density, weighs less than 7kg, and reaches the lightest level in the industry (less than half the weight of comparable products). Five voltage models are available for selection: 0-10V/500A, 0-20V/250A, 0-30V/170A, 0-300V/17A, and 0-600V/8.5A. These models are available with constant current and constant voltage. They operate in constant power mode and provide internal impedance simulation.They can accept three-phase 170 to 265Vac, 342 to 460Vac, or a wide range of 342 to 528Vac inputs, and have active power factor correction.Work efficiency up to 93%.
Cooling fans used in servers and other applications must have the characteristics of small accumulation, high speed, and accuracy. The speed feedback method can be used to achieve the best consistency and suppress fluctuations in the speed caused by supply voltage and load changes. As of now, this method requires the use of a microcomputer, and Toshiba's new solution integrates non-volatile memory (NVM) to enable flexible speed control without the need for an external microcomputer. It also allows easy system configuration.
Corresponds to 3.5V to 4.45V Charging Current Channel Function for 1-Cell Li-Ion Battery Charger IC
Vishay's new FRED Pt Ultrafast rectifiers dramatically increase power density, performance efficiency, and device reliability. These 200V devices are available in automotive and commercial/industrial versions. They are less than 1mm high and can achieve up to 8A single-cathode configurations.
Diodes today introduced the state-of-the-art transient voltage suppressor (TVS) DESD3V3Z1BCSF-7. This product is suitable for advanced system single chip with differential signal line and frequency of 5 Ghz or more. It can provide excellent TVS/ESD protection for I/O port. It is USB 3.1/3.2, ThunderboltTM 3, PCI Express® 3.0/4.0, High-speed interfaces such as HDMI 2.0a and DisplayPortTM 1.4 are integral components.
Silicon Labs (also known as "Core Technology", NASDAQ: SLAB) has introduced a new Wi-Fi® product portfolio, designed to simplify the design of power-sensitive battery-powered Wi-Fi products, including IP security cameras, Point- of-Sale (PoS) terminals and consumer health care equipment. The new WF200 transceiver and WFM200 module support 2.4GHz 802.11 b/g/n Wi-Fi, optimized for energy efficiency, and provide the high performance and reliable connectivity required for ever- Increasing connected devices in home and business networks.
ON Semiconductor (ON Semiconductor, Nasdaq: ON), which promotes energy-efficient innovation, announced the introduction of the latest USB-C (Type-C) series devices, fully compliant with the latest revised specification 1.3, allowing designers to easily integrate USB-C system. The new device includes two controllers and a switch specifically targeted at applications such as smartphones, tablets and notebooks, as well as industrial and automotive use cases.
As more insurance companies launch financial incentive plans, consumer demand for security cameras is also increasing. Auto manufacturers recognize this and begin to use the driving recorder as a factory standard. The first model equipped with an OEM driving recorder has been launched.
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess