EN
  • EN
  • DE
RSS

Blog

Recently, Vishay Intertechnology, Inc. (NYSE: VSH) announced that it will increase the operating temperature range of its HOTcap® K...H series automotive grade radial lead multilayer ceramic chip capacitors (MLCC) to +200°C. The industry's highest temperature for Type II ceramic via devices.
Ams AG, the world's leading supplier of high-performance sensor solutions, today announced the launch of the AS3956, a dynamic NFC tag IC that meets industrial-grade quality standards for mission-critical applications and has a long-lasting lifetime The product offers extremely high reliability.
With the rise of automotive infotainment systems, automakers need to establish reliable and intelligent connections between car displays and multiple smartphones or tablets. Microchip Technology Inc. is the industry leader in providing integrated circuits (ICs) that support this type of connectivity. The five new USB 2.0 smart hub ICs introduced provide users with a variety of options. These devices have a variety of architectures that can be flexibly adapted to the automotive manufacturer's design needs and meet the consumer's easy-to-use and intuitive requirements for the system.
Ams AG, the world's leading supplier of high performance sensor solutions, today introduced the new PCap04, a configurable capacitive sensing front end that enables sensor manufacturers to balance speed and resolution to match their designs demand.
Recently, Vishay Intertechnology, Inc. announced that it has introduced two new high speed silicon PIN photodiodes with enhanced visible light sensitivity - VEMD5510C and VEMD5510CF - to meet the demand for reliable signal detection in wearable devices, medical and industrial applications. Vishay Semiconductors VEMD5510C and VEMD5510CF have filters that suppress infrared radiation and black packages that increase signal-to-noise ratio. They feature fast switching times and small capacitance in a small-sized top-view surface mount package.
Melexis, a global microelectronics technology company, announced the launch of its second-generation motor position sensor (degoker) based on its patented Triaxis Hall magnetic sensing technology.
Vishay Intertechnology, Inc. announced that it has introduced 13 200V to 600V FRED Pt® ultra-fast recovery rectifiers. Both are available in the eSMP series SlimDPAK (TO-252AE) package. Each product has an automotive grade and a commercial/industrial grade. Vishay Semiconductors rectifiers are thinner, have better thermal performance than traditional DPAK (TO-252AA) devices, have higher power density and higher efficiency, and can be used in automotive and communications applications.
Microchip Technology Inc. announced that two new 8-bit microcontroller (MCU) products have been added to the PIC18 product line. These microcontrollers use the controller area network (CAN) bus in conjunction with a number of core-independent peripherals (CIPs) to enhance system functionality. Moreover, designers can more easily develop CAN-based applications without adding complex software. Applications.
Renesas Electronics Corporation, a leading global supplier of semiconductor solutions, announced today that it has expanded its popular RX65N/RX651 microcontroller (MCU) family of products to meet the higher security requirements of industrial automation, building automation and smart metering systems demand. The extended microcontroller integrates Trusted Secure IP (TSIP) and enhanced reliable flash functions and Human Machine Interface (HMI) for industrial and network control systems.
Littelfuse Corporation today announced the launch of two AEC-Q101-compliant transient-suppression diode array (SPA® diodes) families. The AQHV and AQHV-C series are designed to provide extremely fast-acting, high-performance overvoltage protection devices that are best suited for power interfaces, passenger charging interfaces, and LED lighting modules and low-speed I/O.
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess