Terex Semiconductor Co., Ltd. has developed a coil-integrated "micro DC/DC" converter supporting the negative voltage output and the XCL301 series.
Littelfuse Corporation today introduced the smallest series of tubular fuses available on the market. Its rated current is 40A to 63A when the AC voltage is 500V, and the breaking current is 2,000A when the AC voltage is 500V. With a 10mm x 32mm body, the board space required for a single 606 fuse is less than the design of many low-current-rated fuses in parallel. As a result, designers can reduce the amount of board space reserved for protecting components when designing high-power devices.
The B32370* to B32374* series of capacitors have a rated voltage range of 250 VRMS-600 VRMS and a capacity range of 5μF to 600μF. The maximum current capability of different types of capacitors covers 15A to 60A. Capacitors range in diameter from 40 mm to 136 mm and heights from 64 mm to 265 mm. The newly introduced capacitors are extremely reliable and have a service life of up to 100,000 hours. The capacitor uses a synthetic resin as a filler material and does not contain PCB harmful substances. This design makes it possible to continuously operate at a temperature of 70°C. Products are in line with IEC 61071-1 standards, and passed the UL certification.
Analog Devices, Inc. (ADI) announced the introduction of the Power by LinearTM LTC2972, a dual-channel power system manager that monitors the current, power, and power consumption of intermediate bus inputs to point-of-load (POL) converters. Monitoring board power and energy usage is the first step in managing, optimizing, and reducing power consumption. It is designed to reduce server rack and data center cooling and utility costs. The LTC2972 adds software-based, comprehensive monitoring and control to power systems on FPGAs, ASICs, and DSP circuit boards, accelerating time to market, improving system reliability, and optimizing board power consumption.
Renesas Electronics Corp. (TSE:6723), the world's leading semiconductor solutions provider, announces the availability of three programmable power management ICs, the ISL91302B, ISL91301A, and ISL91301B, that provide the most efficient application processor for smartphones and tablets. Power management, while having the smallest board size. Several of these power management ICs also provide power management for artificial intelligence (AI) processors, FPGAs, and industrial MPUs. They are ideally suited for solid-state drives (SSDs), optical transceivers, and various consumer electronics, as well as industrial and networking equipment. Each load in the power supply. The ISL91302B single/dual output multiphase power management IC can deliver up to 20A of output current and 94% peak efficiency in a 70 mm2 solution footprint (more than 40% smaller than similar competing power management ICs).
Littelfuse, Inc. today announced the launch of a family of surface mount fuses rated for up to 1500A of breaking current, suitable for high voltage automotive applications up to 350VAC or 450/500VDC. The size of the 885 series fuses is only 10.86mm x 4.78mm, which is the smallest size surface-mount fuse on the market for 450/500VDC automotive applications. This series of products are limited in circuit board space and are not suitable for applications with traditional through-hole fuses. Ideal choice. The 885 series is rated from 1A to 5A.
Intersil, a subsidiary of Renesas Electronics Corporation (TSE: 6723), a leading global semiconductor solutions provider, today announced the launch of the industry’s first full-HD LCD video processor specifically designed for automotive applications, connected to the latest generation of automotive SoCs ---TW8844. The highly integrated TW8844 builds on Intersil’s industry-leading automotive infotainment and display systems, and is the first high-definition (HD) 1080p LCD video with an analog video decoder, two scalar, and MIPI-CSI2 SoC interfaces. processor.
Sensor development kits from Infineon will significantly reduce design effort, thereby reducing development time and system costs. In order to achieve fast and reliable speed measurement, Infineon Technologies AG has introduced a new Hall sensor TLE4922 and its companion "Speed Sensor 2Go" design kit. The TLE4922 was developed specifically for industrial and automotive applications where fast and reliable speed measurement is critical, such as speed detection of crankshafts and gearboxes in two-wheelers and tricycles. Industrial applications include production and building automation and speed monitoring of electric drive control devices.
Silicon Labs (also known as “Core Technology”) has expanded its energy-efficient industrial-grade microcontroller (MCU) EFM32® Gecko product portfolio to provide higher performance, more features and lower power consumption.
Allegro MicroSystems, LLC announced the release of two new N-channel power MOSFET driver ICs that can control MOSFETs connected in a half-bridge configuration. Allegro's A4926 and A4927 are designed for automotive applications with high power inductive loads and are suitable for DC pumps (brake, oil, water and fuel), HVAC, solenoids and actuators. . These devices are particularly suited for automotive systems that must meet ASIL requirements. Like all other products in the Allegro A2SILTM family, the A4926 and A4927 have integrated enough features to complete the system design and help users achieve the required ASIL level requirements.