EN
  • EN
  • DE

RSS

Blog

Maxim introduces the MAX77756 24V, 500mA, low quiescent current (Iq) buck converter, providing developers of multi-cell, USB Type-C products with flexible options for higher current, dual input and I2C support.
The S8016xA series of SCR switching thyristors provide excellent AC processing and surge stability, enabling them to handle up to 16 ARMS of Class 1 charging at 120V, up to 16ARMS at 100°C and 240V, and up to 25ARMS at 80°C. Level 2 charging. The S8016xA family is the first SCR switching thyristor series capable of handling such high current levels. It is available in TO-220R and TO-263 packages, meets AEC-Q101 requirements, and supports the Production Part Approval Process (PPAP).
Linear Technology Corporation, a division of Analog Devices, Inc. (ADI), introduced the LTC5552, a double-balanced mixer that delivers best-in-class bandwidth matching from 3 GHz to 20 GHz. This mixer can be used as an upconverter or downconverter. The LTC5552 is ideal for upconversion applications because its differential DC port supporting DCs makes the LO close to RF in frequency. Its low LO to RF leakage (less than –25dBm) greatly reduces the burden on the external filter. In addition, this mixer has excellent linearity: 20.1dBm IIP3 at 14GHz and 18.3dBm IIP3 at 17GHz. The device integrates a wideband LO buffer that requires only 0dBm of drive power and virtually eliminates an external high-power LO amplifier circuit. All of these features minimize external components, simplify design and achieve very small solution sizes.
A wide range of EPCOS varistors operate between 11VRMS and 1100 VRMS and can withstand up to 20kA (8/20μs) of inrush current, depending on the model.
Recently, the global Internet of Things promoter Telit announced the launch of the LM940. This is the world's first Full PCI Express Mini Card (mPCIe) module for routers and gateways, supporting LTE Advanced Cat 11, speeds up to 600 Mbps, and will be licensed by mobile network operators in the fourth quarter of 2017.
Intersil, a leading global semiconductor solutions provider, today announced the launch of two new high-speed isolated RS-485 differential bus transceivers, the ISL32741E and ISL32740E, for industrial Internet of Things (IIoT) networks. 40Mbps two-way data communication. Offering up to 1,000 VRMS operating voltage and 6kV of enhanced isolation, the ISL32741E is more than twice as powerful as competing solutions to meet the higher operating voltages and enhanced isolation required by today's most demanding medical and high-speed motor control applications; with 2.5kV isolation The capability and 600VRMS operating voltage of the ISL32740E is the industry's smallest package that enables programmable logic controllers (PLCs) in factory automation applications to achieve high channel densities.
ROHM, a world-renowned semiconductor manufacturer, develops a 48V power-driven in-vehicle system such as a mild hybrid vehicle, and develops the industry's highest step-down ratio of the built-in MOSFET step-down DC 疍C converter under the 2MHz operating (switching) condition. BD9V100MUF-C".
Analog Devices Inc. (ADI) announces the Power by LinearTM LTM8005 step-up DC/DC μModule® (power module) regulator, which is designed to drive LEDs. The LTM8005 places a DC/DC controller, power switch, Schottky diode, and current sense resistor in a 9mm x 11.25mm x 2.22mm BGA package. The LTM8005 operates from an input voltage range of 5V to 38V and delivers up to 1.6A of regulated current at output voltages up to 38V. An external inductor is used, allowing the LTM8005 to be easily configured in different operating modes with a single coupled inductor, including boost, buck-boost, buck, and SEPIC topologies.
NXP's new 3 x 3 x 0.9 mm package S08 MCU further expands its S08 MCU product family to meet the broad market demand for miniature 8-bit MCUs
ROHM, a world-renowned semiconductor manufacturer, has developed the MI sensor "BM1422AGMV" for detecting geomagnetism in the field of vehicle detection for parking lot vehicle management systems.
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess