Analog Devices, Inc. (ADI) announces the LTC6363-0.5, LTC6363-1, and LTC6363-2 precision, fixed-gain, fully differential amplifiers, an ultra-precise fixed-gain version of the proven LTC6363 amplifier. The new products offer fixed gains of 0.5, 1 and 2V/V, providing the flexibility to adjust the input to the ADC full scale.
Ajay Srikrishna, vice president of Cypress's Wired Connections division, said: "With the popularity of USB-C applications this year, the demand for USB-C power will increase. This puts more pressure on our customers. Need to quickly bring power adapters, mobile phone chargers, car chargers and mobile power to the market while keeping up with the fast-growing USB standard. Our highly integrated EZ-PD CCG3PA controller is designed to simplify USB-C power products The requirements are optimized to support not only the required charging standards, but also to keep up with the development of technical standards through firmware upgrades."
Microchip Technology Inc. has introduced a new line of low-power microcontrollers (MCUs) for driving liquid crystal displays (LCDs), integrating core-independent peripherals (CIP) and intelligent analog. The PIC16F19197 family of nine devices includes a battery-friendly LCD-driven charge pump, a 12-bit analog-to-digital converter with computational power (ADC2), a low-power comparator, and an active clock tuning feature for the high-frequency oscillator. They are the first 8-bit MCU family optimized for the popular low-power, battery-powered, touch-enabled LCD applications.
Melexis today announced a new line of magnetic latches and switch sensors that are the world's first to integrate two silicon dies in the same package. These extremely reliable devices are designed for automotive applications including gearboxes, power steering, brakes and locks/latches, marking a significant advance in magnetic induction technology.
NXP Semiconductors N.V. (NASDAQ: NXPI) today introduced the industry's first 12V smart audio amplifier TFA9892. Combining power and compact form factor, this audio amplifier combines high output power, high efficiency and excellent drum resilience for deeper bass so that it can be used for smartphones, netbooks and sound bars. All kinds of electronic equipment bring extraordinary sound quality.
Diodes' DPS1133 single-channel power switch is the world's first high-voltage power switch designed to meet all the stringent protection and fast-use switching needs of USB Type-CTM ports. This product is suitable for a wide range of mobile and desktop computing devices and peripheral devices, as well as consumer electronics, mobile communications, industrial and medical markets, such as smart phones, AR / VR glasses, robots, Car infotainment and home appliances.
Fujitsu Electronic Components (Shanghai) Co., Ltd. announced today that it has introduced a new FRAM (Ferroelectric Random Access Memory) solution - MB85RS128TY and MB85RS256TY, which are the first devices in this new product line. Operating in high temperatures up to 125 degrees Celsius, these devices are designed for the automotive industry and industrial control machinery with motors installed and meet the stringent automotive industry AEC Q100 standards. Fujitsu Electronics hopes to expand its automotive market applications through this new product line and support innovative product development projects.
Teledyne e2v, a company brand of Teledyne Technologies and a global leader in innovative imaging solutions, recently announced the Emerald 67-megapixel image sensor, adding a new member to the Emerald CMOS image sensor family. With a high resolution and the smallest global shutter pixel (2.5μm) on the market, this new sensor is capable of capturing more objects with a single high-resolution image, making it ideal for high-end automated optical inspection, microscopy and monitoring.
Analog Devices Inc. (ADI) announces the Power by LinearTM LTC7862, a high efficiency switching surge suppressor with overvoltage and overcurrent protection for high availability systems. The LTC7862 drives an N-channel power MOSFET stage. During normal operation, the LTC7862 delivers input voltage to the output with very low conduction losses. At input overvoltage conditions, the LTC7862 acts as a high efficiency DC/DC regulator startup switch to protect critical downstream components by limiting output voltage and current.
One of the world's largest satellite communications operators, Eurostar (NYSE and Paris Stock Exchange: ETL) and STMicroelectronics, the world's leading MEMS supplier across multiple electronic applications, the world's leading semiconductor supplier STMicroelectronics, ST for short; New York Stock Exchange (STM) code: STM announces significant results in the development of next-generation satellite chips, which will be used in European satellites' SmartLNB interactive satellite terminals.