Linear introduces the μModule® (micromodule) integrated isolated AnysideTM switch controller LTM9100, which protects and monitors high voltage DC power supplies up to 1000V. High voltage power supplies for industrial, datacom, avionics, and medical applications require controlled turn-on and isolation to control circuit protection, operator safety, and ground ground.
Dialog Semiconductor, a provider of highly integrated power management, AC/DC power conversion, solid state lighting (SSL) and Bluetooth low energy (BLE) technology, is introducing the next generation of its SmartBond family, the DA14586. The new system-on-chip (SoC) is the company's first stand-alone device to support the latest Bluetooth 5.0 specification, providing the lowest power and unparalleled functionality for advanced applications.
Linear introduces the LTC4368 circuit protection controller, which guarantees safe voltage and current levels for 2.5V to 60V electronics in battery-powered automotive, industrial and portable systems.
Linear introduces the H-grade version of the LT8304/-1, a monolithic flyback regulator that guarantees operation with junction temperatures up to 150°C. By sampling the isolated output voltage directly from the main-side flyback waveform, these devices can be regulated without an optocoupler or a third winding.
STMicroelectronics (ST; New York Stock Exchange: STM) announced that its STSAFE family of security units has added a powerful plug-and-play solution for Sigfox low-power wide-area Internet of Things (LPWAN) devices. Provide advanced security features.
ON Semiconductor (Nasdaq: ON), this year's Embedded World show will focus on the electronics industry's three most prominent and fastest-growing areas, demonstrated in the Internet of Things (IoT), Wireless and USB Type-C power/charge, as well as solutions and tools for car image sensing.
Microchip Technology Inc. has recently expanded its AVR® microcontroller (MCU) product line to introduce three new tinyAVR® MCU families. The advent of new ATtiny1617 family of MCUs has enabled the AVR family with core-independent peripherals (CIP) to grow, helping to increase system throughput and reduce overall power consumption.
Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today introduced the IR3883, an easy-to-use, fully integrated, high-efficiency DC-DC regulator designed for energy efficiency, reliability and thermal management High density point of load application. The device is ideal for networking, telecom, server and storage solutions.
Maxim's MAX17222nanoPower boost (boost regulator) delivers the industry's highest efficiency and 300nA minimum quiescent current (IQ), helping wearable and consumer IoT designs achieve maximum battery life in the smallest area.
Vishay Intertechnology, Inc. (NYSE: VSH) announced the launch of its new AEC-Q200-certified ultra-thin, high-current IHLP® inductor, the Vishay Dale IHLP1616BZ-5A. With an external dimensions of 1616, the inductor can operate at +155°C and has a thickness of only 2mm, saving space in automotive applications.