EN
  • EN
  • DE
RSS

Blog

Linear introduces the μModule® (micromodule) integrated isolated AnysideTM switch controller LTM9100, which protects and monitors high voltage DC power supplies up to 1000V. High voltage power supplies for industrial, datacom, avionics, and medical applications require controlled turn-on and isolation to control circuit protection, operator safety, and ground ground.
Maxim Integrated introduces the MAX30034, the latest defibrillation protection device, for use in medical devices such as defibrillators, ECG (electrocardiogram) diagnostics and monitoring, from defibrillation pulses and electrostatic discharge (ESD). Compared to existing processing methods and devices, the device simplifies design, saves more than 75% of space, reduces bill of materials, and dramatically improves performance.
Linear introduces the LTC4368 circuit protection controller, which guarantees safe voltage and current levels for 2.5V to 60V electronics in battery-powered automotive, industrial and portable systems.
Linear introduces the H-grade version of the LT8304/-1, a monolithic flyback regulator that guarantees operation with junction temperatures up to 150°C. By sampling the isolated output voltage directly from the main-side flyback waveform, these devices can be regulated without an optocoupler or a third winding.
Maxim announces the MAXREFDES155# DeepCover® embedded security reference design to help users quickly and easily add confidential security authentication to their systems, protecting Internet of Things (IoT) hardware and the authenticity and integrity of device-to-cloud data exchange.
ON Semiconductor (Nasdaq: ON), this year's Embedded World show will focus on the electronics industry's three most prominent and fastest-growing areas, demonstrated in the Internet of Things (IoT), Wireless and USB Type-C power/charge, as well as solutions and tools for car image sensing.
Intersil, a leading global semiconductor solutions provider, Renesas Electronics Corporation (TSE: 6723), today announced the availability of the ISL94202 3- to 8-cell battery pack monitor to support applications such as vacuum cleaners, lawn trimmers, handheld power tools, and electric Systems that require lithium-ion batteries and other chemical batteries, such as bicycles, scooters, electric toys, and electrical energy storage.
Infineon Technologies AG (FSE: IFX / OTCQX: IFNNY) today introduced the IR3883, an easy-to-use, fully integrated, high-efficiency DC-DC regulator designed for energy efficiency, reliability and thermal management High density point of load application.
Vishay Intertechnology, Inc. (NYSE: VSH) announced the launch of its new AEC-Q200-certified ultra-thin, high-current IHLP® inductor, the Vishay Dale IHLP1616BZ-5A. With an external dimensions of 1616, the inductor can operate at +155°C and has a thickness of only 2mm, saving space in automotive applications.
TDK Corporation (Tokyo Stock Exchange: 6762) has recently expanded its EPCOS ThermoFuseTM product family with the introduction of the new compact NT14 and NT20 series of thermal fuse-protected varistors. The new ThermoFuseTM components take up little space to meet the layout requirements of today's boards.
RFQ RFQ RFQ BOM BOM BOM API API API Sell Sell Sell your Excess