STM32L4 B-L475E-IOT01A Development Kit Integrates high-performance, ultra-low-power STM32L4 microcontrollers with wireless communication modules such as BLE, Sub-GHz and Wi-Fi on a single board, and dynamics with printed antennas NFC tag IC.
The HVC series is especially suitable for battery management systems and DC charging stations in the field of electric vehicle applications. It is widely used in DC traction systems, photovoltaic systems, energy storage systems, and uninterruptible power supplies Applications.
The TDK Group has expanded its range of EPCOS film capacitors for DC links. The newly expanded B3277*H series is suitable for harsh environmental conditions and has been tested for 1000 hours of temperature and humidity (THB) at an ambient temperature of 60 ° C, 95% relative humidity and rated voltage. Extremely stable. Of course, for other special models, we also performed a 1,000-hour THB test at an ambient temperature of 85 °C, a relative humidity of 85%, and a rated voltage.
TDK has expanded the EPCOS 3-wire EMC filter B84243*'s product range to include 10 filters with currents up to 280A. All 18 filters in this series have a rated voltage of 530VAC. The performance of this series of filters is optimized for EN 61800−3:2004+A1:2011 motor cable limits up to 25m (C1) or 50m (C2).
TI Introduces Stackable 16V Input, 40A SWIFTTM DC/DC Buck Converter with Innovative Control Topology
PiTime's executive vice president of marketing at SiTime, Piyush Sevalia said: "SiTime is focused on solving difficult timing challenges. The SiT9005 programming spread spectrum oscillator ensures radiation compliance without the need for costly troubleshooting, redesign, or re-encapsulation. Speed up product revenue."
As China's leading supplier of RF and mixed-signal chips, Vimicro's RDA Microelectronics (RDA) announces the launch of a single-chip RDA5836 high-performance Bluetooth audio system with ultra-high performance and ultra-low performance. The characteristics of power consumption, the introduction of the Bluetooth headset market leader.
Microchip Technology Inc. announced today that it is providing the industry's first external CAN Flexible Data Rate (CAN FD) controller. With the MCP2517FD, designers can quickly upgrade from CAN 2.0 to CAN FD, benefiting from the CAN FD enhancement protocol.
Linear Technology Corporation, a member of Analog Devices, Inc., introduced the 25A step-down μModule® (power module) LTM4645, which can be used in multiple independent devices (N). The current is divided equally between at least one LTM4645 for backup (+1) to ensure power availability when a device in the N+1 configuration detects a fault and must be disconnected. For example, a 75A, 1V load such as an ASIC requires 3 LTM4645s to provide a total of 75A (= 3 x 25A) current. To provide system resiliency, an additional LTM4645 was added as a 3+1 form backup, resulting in four LTM4645s sharing the current to provide 75A in the event of an LTM4645 failure.
Recently, Vishay Intertechnology, Inc. (NYSE) announced the launch of its new 2A to 10A device, the SiC46x, with an input voltage of 4.5V to 60V, and expanded its microBUCK® synchronous buck regulator. The Vishay Siliconi × SiC46× device is space-saving, combining a high-performance N-channel trench MOSFET and a controller in a small MLP55-27L package for high efficiency, high power density and long-term reliability. Simplified thermal management.