Recently, Vishay Intertechnology, Inc. (NYSE: VSH) announced the launch of a new series of ruggedized ENYCAPTM electrical double layer energy storage capacitors, the 225 EDLC-R ENYCAP, for energy harvesting in harsh, high humidity environments. And backup power. Vishay BCcomponents 225 EDLC-R ENYCAP is the industry's first product to achieve a lifetime of 2,000 hours at +85°C. It has been tested with live 85/85 1000 hours and has the highest resistance to moisture.
James Wilson, senior marketing director of clock products at Silicon Labs, said: "Ultrafast data centers are rapidly migrating from 10G to 25G, 50G and 100G Ethernet to accelerate data transmission and increase network efficiency. This new wave of investment cycles has prompted equipment manufacturers to switch Upgrade access ports to higher speeds and use higher-performance clock solutions. By choosing Silicon Labs' Si5332 arbitrary-frequency clock chip, system designers can optimize their clock tree design without compromising clock performance."
Recently, Global Internet of Things Promoter Telit announced that VAIO has selected the LTE Type 9 (Cat 9) LN940 mobile data card from the Telit LN940x product line to provide reliable and secure LTE-Advanced connectivity for its S-series notebooks for mobile professional users. . As a global single SKU (single bar code) solution for OEM streamline logistics, inventory management and global deployment.
Silicon Labs (also known as "Coretech") announced a series of industry's lowest jitter, highest integration, lowest power clock generator products for PCI Express® (PCIe®) Gen 1/2/3/4 applications. . Developers can now confidently design a PCIe-compliant solution using Silicon Labs PCIe clocks, and get maximum jitter margins and reduce product development risk.
Linear Technology Corporation, a member of Analog Devices, Inc., introduces the μModule® step-down regulator LTM8065, which accepts up to 40V input voltage (42V) Absolute Maximum), which safely operates from an unregulated or fluctuating 12V to 36V input supply in noisy environments including industrial robots, test and measurement, medical, factory automation, and avionics systems .
Currently, the market is increasingly demanding more accurate water meters and remote meter readings, and new MCUs and reference designs can provide corresponding support to achieve efficient water resource management, accurate measurement, and timely billing.
ROHM, a world-famous semiconductor manufacturer, has developed an automotive grounding operation with an overwhelming EMI tolerance*1) (hereinafter referred to as "anti-noise performance") for core systems such as EV / HEV engines and automotive electronic systems using on-board sensors. Amplifier "BA8290xYxx-C Series" (BA82904YF-C / BA82904YFVM-C / BA82902YF-C / BA82902YFV-C).
Intersil, a subsidiary of Renesas Electronics Corporation, a leading global semiconductor solutions provider, announced today the introduction of the industry’s first tablet, ultrabook, mobile power and other mobile devices that use reversible USB Type-CTM connectors. Buck-Boost Regulators - ISL95338. This new bi-directional regulator accepts a wide range of DC power inputs, including AC/DC power adapters, USB PD 3.0 ports, travel power adapters, mobile power supplies, etc., and converts power to a stable voltage up to 24V . The ISL95338 also converts a wide range of DC power supplies at the adapter input to a stable 20V voltage.
ON Semiconductor, which promotes energy-efficient innovation, has introduced two new highly-integrated one-megapixel (Mp) CMOS image sensing products to advance the company's significant progress in the rapidly growing field of automotive imaging. The new device provides a complete solution that integrates image sensor and processing functions in a low-power system-on-a-chip (SoC) to simplify and accelerate adoption in applications such as rear view and look-around cameras. Compared with the traditional solution consisting of discrete sensors and processors, its PCB space has been reduced by more than 30%. This assists designers in implementing camera solutions without affecting the shape and aesthetics of the car.
Linear Technology Corporation, a member of Analog Devices, Inc., introduced the 25A step-down μModule® (power module) LTM4645, which can be used in multiple independent devices (N). The current is divided equally between at least one LTM4645 for backup (+1) to ensure power availability when a device in the N+1 configuration detects a fault and must be disconnected. For example, a 75A, 1V load such as an ASIC requires 3 LTM4645s to provide a total of 75A (= 3 x 25A) current. To provide system resiliency, an additional LTM4645 was added as a 3+1 form backup, resulting in four LTM4645s sharing the current to provide 75A in the event of an LTM4645 failure. Applications that can benefit from the N+1 redundancy features of the LTM4645 include data centers, aerospace, banking transactions, and cloud systems, where improving system security and integrity is a top priority.